Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Secondary Side Switch-Mode Power Supply Control Slide 4

The circuit shown on this slide has voltage control loop implementation, sensing the voltage across the voltage divider on the output of the power supply and driving the optocoupler to provide feedback to the primary side controller. The optocoupler provides an isolation barrier of up to 2,500 volts of isolation. This allows for providing feedback to the primary side without ever having the possibility of the high voltage on the primary side ending up on the secondary side, presenting a shock hazard to the user or damaging the electronics on the secondary side. Therefore, an optocoupler, which ST does not provide, is used as part of the feedback loop with the CV/CC controller. What the device provides is the constant voltage and constant current control signal that is fed back through the optocoupler which provides an isolation barrier similar to what a transformer does.

PTM פורסם ב: