Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Thermal Interface Product Selection Slide 14

It is also critically important to analyse the device footprint when selecting a TIM. When working with a large device, a gap filler or putty is likely to provide better performance as it will conform easily to any surface irregularities and fill all voids and interstices of the product. This ensures a good thermal transfer will be achieved. A putty can be especially effective when working with a rough mating surface. This is due to the fact that it can be highly compressed without placing significant pressure on sensitive components. For low footprint devices however, a grease or a phase change material will often times be more effective.

PTM פורסם ב: