Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Thermal Interface Product Selection Slide 18

The surface area of the device is also an important factor in the selection of a TIM. Highly machined surfaces, such as those found in military and some aerospace applications, will allow almost any TIM to be used. However, when working with a rough surface it is important to use a soft gap filler or a putty to ensure that all voids are filled and good thermal transfer is achieved.

PTM פורסם ב: