Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Thermal Interface Product Selection Slide 16

Clamping pressure is also a key design parameter to consider when selecting a TIM. For low clamping pressures, a gap filler is recommended as they are generally soft enough to conform to the surface of a device and provide a low thermal resistance path for heat flow. For higher pressures, a grease or PCM is recommended. When using a silicon based gap filler, too much pressure (say, above 45% compression) can result in silicone oil bleed. This will, under certain conditions, be detrimental to the life time and performance of a device. However, when using a PCM or grease, too low a pressure will prevent a good heat transfer path from being achieved; this could also significantly shorten the working life time of a device.

PTM פורסם ב: