Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Thermal Interface Product Selection Slide 20

If it is likely that the joint will need reworking in the future, it is essential to select a TIM compatible with this requirement. Typically, gap fillers are easier to rework than PCMs or greases. It is generally advised that PCM or grease materials be replaced after a rework to ensure the best long term functionality and device life time. As an added note, PCMs are best removed when slightly warm.

PTM פורסם ב: