Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Thermal Interface Product Selection Slide 4

Phase change materials, or PCMs, are supplied as a solid pad. When a critical temperature is reached, such as during an initial burn in or during the initial use of the device, the pad will melt and begin to flow. As the material flows it will fill the voids and interstices on the mating surface, providing a lower thermal resistance between the mating surfaces. T-Global offers PC99 as their phase change material.

PTM פורסם ב: