Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Thermal Interface Product Selection Slide 17

It is essential to consider the maximum pressure that can be placed on the components. For example, if a BGA is used, the maximum pressure applied must be minimised. In this case, a proper solution would be to use a softer gap filler or a putty. A putty could be especially effective as it can be compressed by as much as 90% with pressures as low as 2 PSI.

PTM פורסם ב: