Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 21

As mentioned, there are multiple versions of SPI, including Simplified SPI (SSPI) and Serial I/O Port (SIOP). As can be seen on this slide these simplified versions have no chip select, intended for use in a single master/slave application. As the name implies, these are much simpler for the user to develop with.

PTM פורסם ב: