Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 7

Not all serial data standards define all seven layers. For example, CAN Bus only defines and uses layers one, two, and seven. However, all seven layers are commonly defined for higher speed serial data standards used in internet data transmission or optical data transmission. In this presentation parts of the Protocol and Application layers will be shown referring to the Physical layer. In other words, the analysis will start from the Phy layer in order to fully decode and understand (at the “Application” level) what is happening on the bus, based on a Phy layer analysis, which is very different from a Protocol analyzer approach.

PTM פורסם ב: