Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 27

On this slide, twenty CRC errors have been captured, and the fourth error waveform is being displayed. Looking at the top row, the fourth packet is highlighted, and it is being displayed in the expanded image at the bottom of the screen. This is an application of the sequence mode; twenty CRC errors are being captured, with any dwell time between them. No memory is being wasted and with the segment function it is possible to look more closely at any of them.

PTM פורסם ב: