Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 37

In the display shown on this slide the scope has been set up to find a runt pulse between the low and high thresholds, with 10% hysteresis, using WaveScan. A red marker has been placed on a pulse that appears to be approximately 30% of the amplitude of other pulses.

PTM פורסם ב: