Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 41

It is important for an engineer to keep complete documentation. In the old days it was done by saving a screen shot; in the really old days a Polaroid camera was used to photograph a display image. Today, LabNotebook is one of the most advanced documentation tools on the market. It allows the user to save the screen shot, the oscilloscope set up, and the acquired data. The information can be saved to multiple destinations including internal memory, hard drive, and external memory. Also with this archiving, the data, the image and the oscilloscope setting, further off-line processing can be done later.

PTM פורסם ב: