Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Embedded Systems Troubleshooting with Oscilloscopes Slide 6

Looking at the waveform on this slide, it can be seen that the ID is overlaid in red, a DLC is overlaid in green, the data values, 6A and 6B are overlaid in blue, the CRC is the darker blue, and at the end is the acknowledge. Using the colored overlays allows the user to easily disseminate the bit values. The oscilloscope is capturing the physical layer of the signal, bringing the data into the machine. The decoders are showing the protocol layer, the hexadecimal, and in certain cases, as in CAN bus for example, they can do symbolic decoding, which is more in the application layer. To summarize, the scope captures the physical layer, and the decoders take care of the rest. The ID in this case is 400, and there are two data values in the frame, 6A and 6B. This will be discussed further in a later slide.

PTM פורסם ב: