Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MLPMLS-Slide11

Heatsinking is simple and effective. The temperature profile shown here shows that with the bottom of the capacitor heatsunk to a fixed temperature, the temperature rise on the top with 5W of power dissipation is no more than 1.8°C. That is a very small thermal resistance of 0.36°C/W.

PTM פורסם ב: