Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MLPMLS-Slide26

While the ripple current handling capability of most aluminum electrolytic capacitors is specified for ambient temperature around the capacitor, for the MLP and MLS the ripple current capability is specified for the case temperature, and is similar to how current capability is specified for semiconductor devices. The previous slide showed Өcc, the core-to-case thermal resistances for MLP and MLS capacitors. The maximum permitted internal temperature for the MLP is 88°C and for the MLS is 125°C. Determine the ripple current capability in the application by calculating the expected temperature rise as shown here. Separately determine the thermal resistance from the case to ambient, Өca. Ripple current capability decreases with increasing rated voltage because of increasing ESR. For the lowest rated voltage the 85°C case, 20kHz ripple current capability for the MLS is 19.9A and for the MLP is 9.8A. For the same rating snap-in capacitor the MLP has about 25% higher ripple current rating and the MLS has about 2½ times.

PTM פורסם ב: