Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MLPMLS-Slide23

The MLS ratings have the 20% voltage derating needed for 125°C operation built in. So, comparing the MLS and MLP ratings shown here, that generally the same capacitance is available in the MLS and the MLP but in the MLS it is at a lower rated voltage. The customer may operate the MLS at the higher MLP rated voltage if the temperature limited to 105°C.

PTM פורסם ב: