Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MLPMLS-Slide24

Continuing the comparison of the MLS and MLP, the internal capacitor elements are the same except the MLS is limited to 250V and is one step lower rated voltage than the MLP. The MLS’s stainless case requires that both the negative and positive leads emerge from the case welded to aluminum rivets mounted in rubber grommets. Thus the MLP has slightly lower inductance with its negative lead welded directly to the aluminum top. Although the MLS’s negative lead is not welded to the case, it is electrically connected to the case by bridging of the conductive liquid electrolyte between the case and the capacitor element.

PTM פורסם ב: