Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide10

Contact erosion, when the contact material itself is actually diminished, should be considered if arcing will occur, particularly if vaporized contact material condenses in the form of powder within the switching unit. Arcing may cause the failure of the contacts to separate, which is called welding and causes the switch to fail in reliably opening the circuit. The correct switch contacts are essential to prevent these problems.

PTM פורסם ב: