Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide24

The IP designation consists of the letters IP followed by two numerals. The first number indicates the degree of protection provided by the enclosure against solid foreign objects entering the enclosure or people being able to open it. The second number indicates the degree of protection provided by the enclosure with respect to the harmful entry of water. The higher the number, the more protected the device.  For example, an IP66 rated enclosure is “dust tight and protected against powerful jets of water from any direction.”

PTM פורסם ב: