Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide18

As mentioned previously, “Cost of Failure” refers to the cost to the manufacturer or end-user of the product if the switching component fails. The cost includes not only the cost of the switch component, but also any additional costs incurred, such as service calls, costs to recall a product, and insurance claims resulting from a failed switch. If dealing with a High Cost of Failure application, Honeywell offers “Premium” V7 series MICRO SWITCH™ devices where the cost to replace the switch and service the failure is significantly higher than the price difference between a premium device and a standard switch. Honeywell’s “Standard” V15 series switch products are useful for low cost of failure applications.

PTM פורסם ב: