Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide11

There are usually several contact options when specifying switches for low energy switching, which is typically defined as less than 12V and lower than 0.4A. Silver contacts easily oxidize and a low-energy arc does not clean the contacts when switched, as does a high-energy arc. For any application where sulfides or moisture are present, silver contacts should not be used unless they are contained within a sealed switch. Sealed switches should also be used if particle contamination of the contacts is anticipated or if a film contaminant such as paint spray or oil mist is present in the application.

PTM פורסם ב: