Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide30

The sixth design factor involves the customer’s requirements for production assembly and servicing. For example, if the surface against which the switch is mounted is warped, rough, or if the mounting screws may be over tightened, that condition needs to be taken into account when helping to specify the device. No matter what the package size needed or the space available for it, Honeywell’s electromechanical switches are ruggedly constructed and can handle considerable abuse if required.

PTM פורסם ב: