Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide19

The third design factor to consider is the physical environment where the switch will be used. Ambient temperatures above those for which the switch is designed can reduce insulation resistance and the dielectric properties of plastics, decrease the elastic modulus of the spring material, and interfere with the efficient cooling of the contacts. Humidity can interfere with contact performance, as can particle or chemical contaminants.

PTM פורסם ב: