Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide9

Another consideration when selecting a switch is whether the circuit may create arcing, as the effect of arcing on contacts is a significant load design factor. There are several distinct consequences of arcing, all of which can affect the type of contacts selected. Sublimation is a situation where material changes from a solid to a vapor and back to a solid. This can obviously have an impact on the contacts themselves if the material from which they are constructed reacts when encountering the solid or the vapor.

PTM פורסם ב: