Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide5

The first task in selection is to determine if the electric circuit requires a normally closed or normally open switch. If the switch is normally open, the switch is not activated in its rest position and there is no current flow. When actuated, the contacts are closed, completing the circuit. When wired as normally closed, the switch is activated in its rest position. When actuated, the contacts are opened and the circuit is broken.

PTM פורסם ב: