Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
protection vrwm
The discussion will now focus on some of the key parameters associated ESD protection devices. The first parameter to be discussed is the reverse standoff voltage VRWM. This parameter specifies the maximum operating voltage on the protected line. VRWM is the breakthrough voltage of the protection diode at which it becomes conductive in the reverse direction, shunting the overvoltage of an ESD strike to ground. The value of VRWM must be greater than or equal to the maximum operating voltage; otherwise the protection diode will become conductive during normal operation and disturb the functioning of the electrical device. However, a small leakage current at operating voltages cannot be prevented; therefore, the maximum leakage current, IRM, at the reverse standoff voltage is defined. The value of the maximum reverse leakage current may of course not exceed the maximum allowed leakage current of the protected application.
PTM פורסם ב: