Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
ic trend esd
In this graphic, the relation between the needed die area of an integrated circuit to implement a function and the die area needed to protect the circuit is demonstrated. Due to the continuous effort to reduce the die area to save costs and the reduction of the gate oxide thickness, the chip size is now less than the 65 nanometer mark shown in the graphic. The disadvantage of the minimized structure is the increased vulnerability to ESD strikes, which results in the die area needed to protect the circuit outgrowing the size of the function itself. Therefore, external protection is strongly needed to protect the circuit against ESD strikes.
PTM פורסם ב: