Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
protection ppp
The protection device has to have the capability to absorb the power generated by a transient voltage; this capability is specified by the peak pulse power, PPP, parameter. It is the product of the maximum peak pulse current and the maximum clamping voltage during an 8/20 µs pulse.
PTM פורסם ב: