Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
broad 100 to 0.4
Another important parameter when choosing the optimal protection diode is the capacitance of the diode. This is especially important for high-speed datalines; for example for USB, HDMI or DVI-port protection. Nexperia offers protection diodes in six different capacitance classes, from standard capacitance to femto Farad capacitance. Each class is labeled with one letter: S for standard capacitance over 50pF, L for low capacitance between 20 and 50 pF, V for very low capacitance from 5 to 20pF, U for ultra low capacitance from 1 to 5 pF, X for capacitance between 0.5 and 1pF, and the recently introduced F-capacitance class for protection diodes with less than 0.5pF total capacitance.
PTM פורסם ב: