Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
clamping hi varistor
As mentioned earlier, the clamping voltage is one of the most important parameters of protection devices since it is a direct measure of the degree of protection for the integrated circuit. In these graphs, the clamping voltage per peak pulse current for an 8 to 20µs pulse is shown for a varistor, on the left, and a Nexperia protection diode, on the right. The clamping voltage for the varistor is clearly higher than for the Nexperia device, therefore increasing the chance of failure for the integrated circuit.
PTM פורסם ב: