Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
General Purpose Motor Drivers in 3-15 Volt Range Slide 10

Another example where motor drivers are commonly found is in the video projector. Most mid-end projectors will have motor driven zoom and focus. In lower-end models, these functions are done manually. When the projector is mounted in a remote place, such as a high ceiling, it is convenient to be able to adjust the zoom and focus without having to get out a ladder. High-end models could include a motor for lens shift and an iris function. Lens shift is the ability to control the position of the lens in all directions. Some projectors have a swivel function, enabling the chassis to move right and left.

PTM פורסם ב: