Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
General Purpose Motor Drivers in 3-15 Volt Range Slide 2

There are many applications for 3-15 VDC motor drivers. These include security cameras, video projectors, toys, and valve control in water and gas applications. The project the designer is working on may not be one of these exact applications, but what is being controlled is probably very similar. This tutorial will take a closer look at some of these applications.

PTM פורסם ב: