Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
General Purpose Motor Drivers in 3-15 Volt Range Slide 22

What about valve control? If precise position and not just on and off are needed, a stepper motor is most commonly used. For on and off, H-bridge drivers for brush DC motors are chosen. There are dual H-bridge parts available, so it is necessary to know how many channels will be controlled. Once the motor type is identified, the supply voltage range and current requirements can be compared to the charts on the previous slides. For the latest information, the designer should check on the web. To further narrow down the selection, obtain the information needed to answer questions four through six.

PTM פורסם ב: