Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
General Purpose Motor Drivers in 3-15 Volt Range Slide 24

The LV8548MC was previously discussed in the security camera example, as well as in the valve control example. It can be used as a single channel stepper motor driver or as a two channel H-bridge DC motor driver. It has a built in low voltage detection circuit and can source 1 A. There is an evaluation board available for this device.

PTM פורסם ב: