Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
General Purpose Motor Drivers in 3-15 Volt Range Slide 15

Motor usage in the lens of cameras is illustrated on this slide. For auto focus, a stepper motor is used. This application requires two lenses, as the figures in the upper right image show. There is a main lens and the focusing lens. By adjusting the position of this lens, the object will come into focus. This requires precision, therefore a 3 to 5 V stepper motor is used. Zoom does not require the precision in position control that focus does, so often a brush motor is used. The lens iris controls how much light gets to the image sensor. A motor is used to make this opening larger or smaller. A stepper or brush motor is used to position the blades that control the size of the opening.

PTM פורסם ב: