Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
General Purpose Motor Drivers in 3-15 Volt Range Slide 8

Shown on this slide is the block diagram of very small remote control car. A forward/reverse brush motor is used to move the steering left and right and to move the wheels forward and back. The LB1836M was used in this toy car because the available board area was so limited, there was only room for one motor control IC. This device can be used to control the motors in toy robot joints.

PTM פורסם ב: