Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide13

A two ball bearing in an axial fan consists of two sets of ball bearings. The dual ball bearings increase the surface area to provide a smooth and consistent operation by reducing the amount of friction produced. This type of bearing is very stable at high temperatures in comparison to other bearing types, but it is weak against shocks to the fan. Noise becomes more of an issue as the bearing ages.

PTM פורסם ב: