Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide4

The three types of fan noise shown in this slide are directly caused by differences in air flow. The sound generation due to uniform and steady aerodynamic force has very weak noise for low speed fans, and depends on fan RPM. This kind of noise is impossible to avoid, although it can be reduced by increasing the number of blades. Steady but non-uniform inlet air flow causes non-uniform aerodynamic forces on the blades as the angular positions change. This is one of the major noise sources of electronic cooling fans. Unsteady flow causes random forces on the blades which spreads the noises created and makes them continuous.

PTM פורסם ב: