Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide15

Hydro dynamic bearings consists of a shaft riding on a pressurized oil pocket held within the bearing. Without having a physical connection from one race of the bearing to the other, this type of fan bearing has low noise and vibration in comparison to the other types and has a long life because there are not any wearable parts in this bearing. Due to the simple construction, hydro dynamic type bearings are less expensive than other bearings.

PTM פורסם ב: