Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide7

Cubic feet per minute (CFM), is the specification used to help determine the appropriate fan to use in a particular situation by measuring the amount of air the fan can move in a certain time frame. CFM is how many cubic feet of air can be moved in one minute elapsed time. Air flow can be computed in two different ways; the first is using an air flow sensor and the second is using the air flow equation shown in the slide; (Q2/Q1) = (RPM1/RPM2), where Q1 is the air flow rate at RPM1 and Q2 is the air flow rate at RPM2.

PTM פורסם ב: