Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide8

Shown on this slide is a graph of air flow performance. Static pressure is used to evaluate the amount of impact various ventilation system components have on the air flow path within a given system. Fans create positive static pressure to move air through a given system while all other components create negative static pressure that causes resistance to air moving through a system. The positive static pressure created by fans equals the negative static pressure created by resistance as air navigates obstacles in the ventilation path. The line on the graph represents a typical axial fan performance. It can be seen in the graph that as pressure increases, the rate of air flow decreases. Standard atmospheric pressure is 100 kPa or 10.2 mm-H20.  

PTM פורסם ב: