Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 10

To pass digital pulses in an electronic circuit requires surprisingly better circuitry than for a one on one comparison of a 2 GHz clock compared to a 2 GHz RF continuous wave signal. The key difference is the sharp rise time of the digital pulse. Correspondingly, the continuous wave RF signal rises gradually relative to the digital pulse. So to electronically compare the frequencies between continuous wave and digital pulses it takes a minimum of 5 harmonics of a sine wave. This is shown here. Note how the leading edge of the sine in the first square wave is separated from the leading edge of the square, but by the fifth harmonic shown in the last digital pulse the leading edge of the sine wave is very close to leading edge of the digital pulse.

PTM פורסם ב: