Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 15

A signal loss of 3 dB is equivalent to 50% loss of signal strength. If signal loss is beyond 3 dB, the signal strength becomes unusable. In the above diagram a pulse is shown being transmitted through a set of contacts with only 50% of the signal being transmitted through the relay.

PTM פורסם ב: