Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 19

Most circuits accept -20dB as a reasonable working level, however some circuits can work with isolation levels below 20 dB. Reed relays typically isolate signals down to -40 dB at lower frequencies (1 MHz to 200 MHz) and fall off to -20 dB in the 2 GHz to 3 GHz range. The diagram shown here illustrates relay contacts where a pulse is incident on one end of the open contacts. Note that a small part of the signal leaks through the contacts at the higher frequencies.

PTM פורסם ב: