Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 4

Semiconductor processors run computers and determine the speed at which they process information. In other words, the heart of the computer is the semiconductor processor or microprocessor. Its clock produces the digital pulses that determine the speed at which information is processed in a computer. A processor running at 2 GHz has its clock producing 2 billion pulses per second. The more pulses, the faster computers will process information. Therefore, there is a continued push to make computers faster and faster by using semiconductor processors with higher clock rates.

PTM פורסם ב: