Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 11

So what do the 5 harmonics mean in the real world? Stated succinctly, to make up a digital pulse it takes a minimum of five harmonics of a sine wave of the same frequency. So if one has a processor with its clock running at 2 GHz, it is processing or producing digital pulses at the rate of 2 billion pulses per second. After adding the five harmonics, this means that electronic circuitry will need to have the capacity to pass 2 x 5 or 10 GHz. If the circuitry was only capable of 2 GHz continuous wave, a 2 GHz pulse would be seriously rounded off to the point where the pulse becomes ineffective in carrying out its information transfer.

PTM פורסם ב: