Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 34

Slew rate is very closely related to rise time. It essentially the delay between an input and an output. For example, consider a reed relay with closed contact with a perfect square wave incident upon the contacts. As the pulse enters the relay there will be a slight increase in rise time before it exits. This change in rise time between the input and the output is measured and considered the slew rate.

PTM פורסם ב: