Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 6

In contrast to DC, RF uses voltages, currents, and wattages that are always changing in any given instant in time. These changes are usually occurring very rapidly in a periodic way or as a wave motion. This wave motion is similar to the wave motion seen when a pebble is dropped into still water. One complete cycle or wave is considered 1 Hz, or a sine wave.

PTM פורסם ב: