Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
RF Reed Relays Presentation Part 1 Slide 13

Insertion loss is considered one of the most important RF parameters. It basically defines the signal loss when going through a component or circuit (a reed relay, for example). It is measured by first passing a signal with known strength down a given copper strip and measuring its signal strength at the beginning and end of the strip; the component is then added to the copper strip and the signal strength at the end is measured and compared.

PTM פורסם ב: