Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide14

Pulse Rating Curves are also included on all of the MOV datasheets. They are a series of straight lines indicating to the user how many times a certain event can take place before the MOV has reached the end of its useful life. This graph shows that a high current event that lasts for a certain time interval will end the life of an MOV much faster than a low current event. For example, the top line that is labeled “1” can survive just one hit of high energy and the bottom line labeled “indefinite” can survive indefinitely. This graph helps explain to the user what kind of lifetime to expect when a certain threat is encountered. If the threat is a 3000A secondary lightning strike, lifetime will typically be less than ten hits. But if the threat is a much lower 100A industrial switching incident, then the lifetime extends to thousands of hits.

PTM פורסם ב: